Search Results for where is this place
Whip Antennas MU 911-X/... - AMPHENOL PROCOM
Mounting can take place exclusively with access from the outside when drilling an 18 mm dia. hole. Mounting can take place from the inside by drilling a 14 mm dia. hole. When mounting in a 14 mm dia. hole, remove the bottom plastic ring of the packing gasket with a sharp cutter.
Model M625B02 Low Frequency Industrial ICP® Accelerometer Installation ...
constant current circuits in place of the diodes, particularly when driving long signal cables (see Section 5). Decoupling of the data signal occurs at the output stage of the signal conditioner. A 10 to 30 µF capacitor coupled with a resistor shifts the signal level to essentially eliminate the sensor bias voltage.
Amphenol at Data Center World Expo May 9 -11
Amphenol will be participating in the Data Center World at Austin Convention Center in Austin, Texas this coming May. The expo will take place at the following times and you can find Amphenol in booth #847.
The Role of Ceramic Bandpass Filters in Modern RF Design - Q Microwave
And you’ve come to the right place. Check out this article if you are curious about how we create RF bandpass filters in-house. Q Microwave is a RF filter company that manufactures ceramic and other types of filters right in the United States. Boasting cutting-edge technology and rigorous quality assurance, our team of dedicated engineers are ...
Model 3741E12200G DC Response Accelerometer Installation and ... - PCB
sockets. Then thread the connector into place by turning the cable connector’s outer shell onto the accelerometer’s electrical connector. 4.1 SCREW MOUNT This mounting technique requires smooth, flat contact surfaces for proper operation and is recommended for .
RF Technology: The Real MVP in Large Scale Sporting Events
Since then, RF technology has found a place in areas other than broadcasting, which alone has evolved substantially in the last century. Communication systems within stadiums, especially those involving wireless connectivity, such as Wi-Fi which utilizes IoT antennas on ISM bands and wireless ticketing devices that use NFC antennas, are among ...
career | Amphenol Global Search | Amphenol
If you are a professional who is seeking to establish a career with a world leader in electronic component manufacturing, Amphenol RF is the place for you. Amphenol RF offers competitive salaries, comprehensive benefits, work/life balance, an outstanding work environment, entrepreneurial spirit and opportunities for growth.
MachineryMate 800 operating guide - Wilcoxon Sensing Technologies
Place the sensor on a rigid part of the machine as close as possible to the desired measurement point (bearing block) using the magnet mount. Press the POWER button again to take the reading. Note: For best results the sensor should be placed gently onto the measurement point by rolling the magnet
Careers | About Us - Amphenol MAO
Production Assembler (Sidney, NY)Amphenol is a worldwide electronics leader and one of the world's largest manufacturers ofinterconnectproducts.Amphenol is listed on the NYSE and a component of the S&P 500 and is a top performing company with an unparalleled history of growth with over 65 businesses throughout the world.Amphenol ...
Series I Lightweight Ground Modules - Amphenol PCD
Interconnect systems optimized for the extensive data transmissions that take place within modern missiles and guided munition systems during flight. Ruggedized products, optimized for performance and endurance in the world’s harshest environments, and engineered to achieve consistently exceptional performance.
CS239A and CS239E T1 Line Repeaters - Charles Industries
Installation and removal of repeaters should be done with care. Do not force a repeater into place. If excessive resistance is encountered while installing a repeater, remove the repeater and check the card guides and connector to verify proper alignment and the absence of foreign material. CAUTION 6. TECHNICAL ASSISTANCE
30-Port Antenna - Amphenol Antenna Solutions
antenna. For RET control, the transparent caps must be in place and locked. The tilt angle indicators always remain visible and the antenna still has manual tilt control (manual override). Do not remove the transparent cap(s) from the antenna. 6888370-3 6888370N-3 6888370-3G 6888370NG-3
Temperature Sensors - Page 2
Thermometrics, Inc., offers one of the most comprehensive ranges of temperature measurement and sensor products in the world today. From chips to value-added assemblies, with temperature ranges from -196ºC to 1150ºC, Thermometrics products play a vital role in measurement, control and protection of industrial and consumer-based applications worldwide.
PCTEL Announces Spectrum Monitoring and Uplink Testing Solution for ...
Customers can contact PCTEL now to place an order for SeeHawk™ Monitor, expected to ship in the fourth quarter of 2022. PCTEL will demonstrate SeeHawk Monitor along with its other solutions for the critical communications industry at the National Association of State Fire Marshals’ NASFM Fire Prevention & Safety Symposium in New Orleans ...
Model 357C91 Charge Output Accelerometer Installation and ... - PCB
STEP 3: Place a small portion of adhesive on the underside of the mounting base. Firmly press down on the assembly to displace any extra adhesive remaining under the base. Figure 4. Mounting Base: Adhesive Installation METHOD 2 - Direct Adhesive Mount For restrictions of space or for convenience, most sensors (with the exception of integral ...
Meet Amphenol at OFC 2023
It is the go-to place to visit and interact with hundreds of manufacturers on their latest products and innovative solutions and to understand on the trends that drive the market. Amphenol is proud to sponsor the Expo Theater II at the event in San Diego Convention Center, CA, from March 7 th - 9 th , 2023 .
Mobile Mounts X-Mount - AMPHENOL PROCOM
Mounting can take place exclusively with access from the outside when drilling an 18 mm dia. hole. Mounting can take place from the inside by drilling a 14 mm dia. hole, in which case the bottom plastic ring of the packing gasket should be removed with a sharp cutter.
NovaSensor NPC-1210 Medium/Low Pressure Sensor
* Order NPC-1210-XXXG-XN in place of NPC-1210-XXXD-XN The code number to be ordered may be specified as follows: NPC-1210 (Low Pressure) Code Pressure Range 10W 10 in H 2O (25 mbar) 001 1 psi (69 mbar) CodeType DDifferential G Gauge Code Lead Configurations 1Up 3Down Code Tube Options LLong SShort
Commercial Aerospace | Markets - Amphenol
Amphenol is a leading provider of high-performance interconnect systems and components to the commercial aerospace market. In addition to connector and interconnect assembly products, we also provide rigid and flexible printed circuits as well as high-technology cable management products.
Ultrasonic Point Level Sensor
it is important to place the Fluid-Trac® PLS sensor’s face in the center of the tank perpendicular to the liquid level and with no obstructions in the beam path to the liquid. Cone Angle Fluid-Trac® PLS mounting that is not perpendicular to the fluid causes a reduction in its sensor performance. As shown in Figure 3, the amount of