Search Results for novastudio setup v3.4.2
ALDC Software Installation Quick Start - Amphenol Antenna Solutions
Setting up the ALDC software involves three steps: downloading, extracting, and then installing. ALDC software v2.0 for Microsoft Windows. The best way to obtain the latest software is to download it from the Amphenol Antennas Web site.
Software Downloads | Support - PCTEL
Download the latest utilities, software, drivers & more for your PCTEL products, devices, and software.
Network Management System and ICB Management System Software User’s Guide
Use this software to manage the Charles ICB. The NMS system consists of PC software which provides a graphi-cal user interface (GUI) used to provision, control, and monitor multiple 360-80 ICBs. The PC communicates through an Ethernet interface.
NMS044 - pcb.com
2.4 Reviewing 831C SLM System Properties for Use With NMS044 ... This enables one person to deliver and set up the system in only a few minutes. The NMS044 can be deployed, before, during, or after you setup the 831C. 3.Remote Connectivity Access and control the system remotely by connecting
Network Switch Software Documentation 09/30/22
Up dated SNMP examples for V3 and MIB usage in section 5 09/08/20 Updated DHC P and VLA N commands 08/27/21 Added command descriptions for GET ARP GET DHCP GET DROP GET LACP GET MULTICAST ... 2.4. Webserver Password = amphenol The web interface provides a single password only field for accessing the web-based status
360-80 SNMP Network Node Manager (NNM) Setup Guide
This document describes how to configure portions of the SNMP NNM (Network Node Manager) to communicate with the E1-S card used in the Charles Industries ICB. SNMP can be used with 3603-86 E1 cards. This document is reprinted to add the secondary E1 controller (3608–85) functionality.
Netpac™ I/O Driver for THE FIX™ - amphenol-sensors.com
Use this driver reference manual to find support requirements, configuration values, and error code descriptions that are specific to this driver. In addition, have your computer, I/O Device, and FIX applications manuals nearby for reference.
Telaire Accessories: Calibration Kits, Enclosures, Software, Cables
Telaire offers four enclosures to expand the Ventostat and Vaporstat installation options: Model T1508 Aspiration Box, Model T1505 Splash Resistant Enclosure, and Model T1551 and T1552 Outdoor Air Enclosures. Windows based VG Graphing Software allows you to easily download your IAQ measurements and customize graphs.
240GT54/nrg240GT54 2 - Holland Electronics
3 All rights reserved. 240GT54/nrg240GT54 Amphenol Network Solutions 6.5.2020 150567 509.926.6000 — amphenol-ns.com.com Table of Contents Section One: Overview ..... 6
Magnetostrictive Liquid Level Transmitters with ... - Temposonics
5.2 Quick start-up procedure 1. Connect +24 Vdc to terminals. 2. Connect data lines to terminals. 3. Connect the PC (or other device) to data lines. (If you are using a PC, use a RS-232 to RS-485 converter. See Note above for more information.) 4. Turn on power to the transmitter. 5. Start the LP Dashboard. Select Com Port and Address. Factory
136-IM Rev F2 10-15-19 - PCB
Up to three (3) Model 136 units can be installed in a 19” rack using ENDEVCO Model 31979 Rack Mounting Kit.
MMS2/3 and Hygromaster 2 - Protimeter
2. Installation instructions can be found at the end of this guide. 3. Once installed double-click on the Protimeter.exe shortcut available on the desktop or click on the Protimeter.exe option from the windows menu to run the Protimeter software. 4. Make sure that the batteries are properly placed in meter. 5.
360-80 T1 Channel Bank RELEASE NOTES - charlesindustries.com
2. T1 Controller (3603) / Secondary T1 (3608) - Cabling - The RJ-45 cable that goes from the T1 primary (RT1) to the secondary unit RJ-45 (P2) needs to be a crossover cable for bypass function to work properly. Meaning pin 1 to 5, 2 to 4, 4 to 2, and 5 to 1. It is possible to set up a D/I
Amphenol Aerospace
Generate recommendations to improve thermal performance. The primary frame was revised to remove fins above the Aldrin and increase pedestal heights to allow for thinner gap pads on the critical components.
Model 080962-01000 2 Channel Transient Recorder Installation and ...
astener laboratory for measuring fastener torque, angle of turn, and clamp load. Ideal for performing fastener analysis, for auditing and certifying power tools, and for testing hand torque wrenches; Model 962 is a cost effective, versatile, and easy-to-use recorder that can colle.
SGX Infrared Gas Sensor Evaluation Kit IR-EK2 User Guide
Set four alarm levels (2 per channel) which drive on-board LEDs and open collector outputs. Log readings of peak-to-peak output signal, gas concentration and temperature using the supplied PC Data Logging Program. Read the Manual! The supplied CD should auto-run on your PC when inserted into a CD drive. Select ‘User Guide’ from the CD menu.
Charles Retrofit Kit 97-002492-A General Description and Installation
using 1/4-20 hex screws and flat washers from the front, with 1/4-20 Keps nuts on the back. Secure the plate back onto the SHRD60. 2. Attach the lower radio/bracket assembly onto the drilled holes on the right side of the central panel using 1/4-20 hex screws and flat washers from the front, with 1/4-20 Keps nuts on the back.
Model 3743G122G Accelerometer, VC, 2g, triaxial, differential, screw ...
2.0 Common Applications and Features The 3700 Series MEMS DC Accelerometers achieve true DC response for measuring uniform (or constant) acceleration and low-frequency vibration . For this reason, they are often used to: • mass. A high natural frequency is accomplished through the Perform ride quality assessments of elevators, automobiles,
Charles Retrofit Kit 97-002491-A General Description and Installation
2.4.4. Complete the Installation 1. Mount the two Airscale radios to the left of the SHRD60 central spine. For each bracket, use four 1/4- 20 hex screws with flat washers through the front of the holes, securing from behind with 1/4-20 Keps nuts. 2. Mount the AWHHF radio to the right of the central spine. Use four 1/4-20 hex screws with flat ...
Model 6634D Signal Conditioner IM6634D - PCB
• Acceleration output - fixed at 50 mVpk/g pk (or 5.0 mVpk/m/s2 pk) • Velocity output - fixed at 100 mVpk/ips pk (or 3.8609 mVpk/mm/s pk) • Displacement output - fixed at 400 mVpk/mil pk (or 15.4436 mVpk/µm pk) • AC Programmable output can be set to: Acceleration – 2 to 200 g pk, Full Scale (20 to 2000 m/s2 pk)