Search Results for error tololant
Proximity Probe Cabling Errors Ebook - pcb.com
Sometimes loading causes a vibration issue with the shaft. When those situations arise, unexpected outages occur that can cost companies millions of dollars. Proximity probes are most commonly checked through the API 670 method of static calibration.
Protocol Manual MH-Series with J1939 Safety - temposonics.com
The error code provides the following codes including internal memory and controller errors, range error, temperature error, no magnet detected, and multiple magnets detected. Each error adds a bit value to the resulting error code:
Installing the Sensor - Amphenol
To ensure an air tight seal, make sure the mounting surface of the duct is clear of dirt or obstructions. Then, attach the pitot tube to the duct with sheet metal screws or rivets.
TN-9 Shunt Calibration of a Strain Gage Sensor - PCB
Shunt calibration is the known, electrical unbalancing of a strain gage bridge, by means of a fixed resistor that is placed, or “shunted”, across a leg of the bridge.
Busbar Deisgn Guide - Amphenol Interconnect Product Corp
tolerance Standard spacer for easy leveling Double spacer for easy leveling and connecting on both sides (snubber...) Tapped spacer for leveling up connecting point Compliance to standards for worldwide use Captive screw for easy and secure mounting Threaded insert for fast connecting Casted link for reducing impedance and cost Standoff spacer with
Model 2271A / AM20 - PCB
Exposure to rapid temperature change greater than 100°F (38°C) per minute may cause the device to produce spurious high frequency discharges for several minutes. Maintain high levels of precision and accuracy using Endevco’s factory calibration services.
ER Series SAE J1772 Charging Cable/Inlet - amphenol-industrial.com
www.amphenol-industrial.com Amphenol 3 AC charging cable with Vehicle Connector and open cable end for charging electric vehicles (EV) with alternating current (AC) via type 1 Vehicle Inlets, for installation at charging stations for E-Mobility (EVSE)
AR - Amphenol Canada
Contact Amphenol Canada for more information at 416-291-4401 • www.amphenolcanada.com 5 ARINC CANADA 404 How to Order 4. CLASS A Non-environmental, standard commercial connector
Thermal Effects of Solder Reflow on RF PCB Connector Design - SV Microwave
measurement error. A .0008” change in the pin height is not substantial enough to cause mechanical or electrical failure in this application. Measurements were also taken around the rim of the connector using a drop gauge to measure how flat the connectors were sitting on the board after reflow. The measurements were only taken after
Application Guide - Amphenol
This accuracy figure is a total error band and includes all errors due to offset, span, linearity and temperature, as illustrated in Figure 2 below. Figure 2: Accuracy of Calibrated NPI-19 Digital Pressure Sensor
AMPHENOL TCS
Recommend using a “Copper Defined” landing pad as opposed to a “Solder-Mask Defined” pad. “Copper defined” better insures a round, accurately located pad – critical to part location tolerance. “Copper defined” pad produces a more reliable solder joint – allowing solder to wrap around the pad edge.
Kaye Validator 2000 - Wired Thermal Validation
For nearly two decades the Kaye Validator 2000 has been the standard for wired Validations systems in the Pharma/ Biotech industry. Thousands of users trust and rely on the accuracy, reliability and proven performance of the Validator 2000.
12 things to consider when selecting an accelerometer
• Typical sensitivity tolerance range from 5% to 20% – A tight tolerance 5% is the best – A wider 10-20% tolerance can be used when the exact sensitivity value can be programmed into the data acquisition equipment – Tolerances are most important if your data collector or online system
MIL-DTL-38999 Series II - JT Connectors - Amphenol Aerospace
Amphenol's MIL-DTL-38999 Series II and commercial JT series connectors meet or exceed the Mil-Spec requirements and are available in aluminum or stainless steel as well as several different finish options. Amphenol is also qualified to the MIL-DTL-27599 specification for Series II connectors.
NUMBER GS-12-1092 PRODUCT SPECIFICATION - Amphenol CS
This specification defines the performance, test, quality and reliability requirements of the DDR4 288P 0.85mm pitch socket. This specification is applicable to DDR4 family DIMM socket of products which provides memory module card to PCB interconnecting. Max. 3.2 Operating Current Rating = 0.75 A/Contact Max.
Selecting Accelerometers for and Assessing Data from Mechanical ... - PCB
What all of these plots show is that at T/T n equal to 5, the peak error of the measured shock pulse is always less than 10%, and for T/T n equal to 10, almost perfect reproduction is achieved. Thus, the “rule of thumb” when selecting an accelerometer or assessing already recorded shock data, is:
T3030 Series Carbon Dioxide (CO2) Sensors | Telaire
Features, specifications, and documentation for the T3030 Series Carbon Dioxide (CO2) Sensors by NovaSensor. Check distributor stock to place an order.
Why Every Engineer Needs a Reliable Lowpass Filter Calculator
Accurate lowpass filter calculations are critical for RF engineers working on aerospace and defense projects. Even a tiny error can result in difficult-to-resolve performance issues.
PCB LOAD & TORQUE: A PCB GROUP COMPANY Load Cell Handbook
Factors such as temperature, the length of wire used to complete the circuit, and gage placement have an effect on the resistance in the bridge, creating an error in the measured values. In precision load cells, these effects are compensated by adding resistance to the bridge.
61083-20-1-4-0-0-LF | Amphenol Global Search | Amphenol
Intrinsically safe vibration transmitter, 4-20 mA output proportional to peak velocity vibration, 0.5 in/sec full-scale measurement range, ±5% tolerance at full scale, operates up to 85°C, top exit 2-pin MIL-C-5015 style connector, certified for use in Class I Division 1 and Zone 0 / Zone 1 hazardous locations