Search Results for tacbeam
PRODUKTPASS | TacBeam as per VG95319-100; -101 - Amphenol-Air LB
TacBeam is a hermaphroditic lens plug connector, insensitive to dust and dirt. This plug connector is qualified as per MIL-DTL-83526/20 and 21. In addition, it is approved as per VG95319-100, and is thus suitable for outdoor applications.
Drawing of the AFSI TacBeam Interface Adapter
TacBeam Interface Adapter 3.00 MATING PLANE O 1.56 Applications • GroundTacticalSystems • Energy • TacticalBroadcastNetworks Features • TFOCA,TFOCA-II ...
TACBEAM - फाइबर ऑप्टिक कनेक्टर्स | एम्फेनॉल सोकैपेक्स
एम्फेनॉल सोकैपेक्स फाइबर ऑप्टिक कनेक्टर tacbeam एक ...
Connectors, Terminals, Cable, Termination Kits, Test Systems, Training
AFSI products include physical contact connectors, termini, cable assemblies, terminations kits, test equipment, systems & training.
RJSwitch UserManual RES-GMC-1S-RJF-TACBEAM 1-0 - Amphenol Socapex
RES GMC 1S RJF TACBEAM rev. 1.0 Page 7 of 11 Last Rev: Jan. 30, 2014 Amphenol – 948, Promenade de l‘Arve – B.P. 29 – 74311 THYEZ Ced ex – France - +33(0)4.50.89.28.00 – www.rjswitch.com Optical Wiring The optical link is established using TACBEAM 4 ways connectors. 2 ways are used for data transmission (Rx and Tx).
PRODUKTPASS | TacBeam as per VG95319-100; -101 - Amphenol-Air LB
TacBeam is a hermaphroditic lens plug connector, insensitive to dust and dirt. This plug connector is qualified as per MIL-DTL-83526/20 and 21. In addition, it is approved as per VG95319-100, and is thus suitable for outdoor applications.
FIBER OPTICS - Amphenol Fiber Systems International (AFSI)
beam (CTOS, TACBeam®) and others. For applications demanding reliability, traceability and the highest level of quality, a complete plug-and-play cable assembly directly from the manufacturer offers the highest degree of confidence. Amphenol cable assemblies are manufactured by expert technicians in our state-of-the-art facilities.
TACBEAM - Sợi quang Connecteurs | Amphenol Socapex
Le connecteur pour fibre optique TACBEAM d'Amphenol Socapex est un connecteur hermaphrodite conçu pour être utilisé dans des environnements sévères. Il est doté de la technologie du faisceau élargi pour une transmission sans contact, avec des options monomode et multimode et jusqu'à quatre canaux. Le connecteur TACBEAM est qualifié M83526/20 et /21, ce qui en fait une solution fiable ...
connector | Amphenol Global Search | Amphenol
6 Part 4: Assembly Process of Terminal and Cable 4.1: Applicable Cable Selection 4.1.1 Only suitable for the PV cable with cooper conductor. Tin coated wire of conductors is recommended. 4.1.2 The cable OD range from ø5.0mm to ø7.8m, the number of conductor strands is from 7 to 140 for 2.5/4.0/6.0mm² connector.
RES-GMC - 扩展光束技术 - 光纤媒体转换器 | Amphenol Socapex
amphenol socapex 媒体转换器 res-gmc 是一款坚固耐用的以太网光纤转换器,采用符合 mil-std 规范的扩束技术。该设备专为在恶劣的军事环境中提供可靠、安全的连接而设计。该转换器支持 stanag 4290、ctos 扩展光束技术和 m83526 tacbeam 扩展光束技术。它还符合各种 mil-std 规范,如针对 emi 的 mil-std-461e、针对 ...
RES-GMC - 확장 빔 기술 - 광섬유 미디어 컨버터 | Amphenol Socapex
Amphenol Socapex 미디어 컨버터 RES-GMC는 MIL-STD 규격을 준수하는 확장 빔 기술을 사용하는 견고한 이더넷 광섬유 컨버터입니다. 이 장치는 열악한 군사 환경에서 안정적이고 안전한 연결을 제공하도록 설계되었습니다. 이 컨버터는 STANAG 4290, CTOS 확장 빔 기술 및 M83526 TACbeam 확장 빔 기술을 지원합니다.
TACBEAM - Συνδέσεις οπτικών ινών | Amphenol Socapex
Ο σύνδεσμος οπτικών ινών TACBEAM της Amphenol Socapex είναι ένας ερμαφρόδιτος σύνδεσμος σχεδιασμένος για να χρησιμοποιείται σε περιβάλλοντα που είναι επικίνδυνα. Διαθέτει την τεχνολογία του φέιζερ για μια μετάδοση χωρίς ...
Connectors | Products - Amphenol
TacBeam is a hermaphroditic lens connector, insensitive to dust and dirt. This connector is qualified as per MIL-DTL-83526/20 and 21. In addition, it is approved as per VG95319-100; -101, and is thus suitable for outdoor applications. A marine bronze version is also available (according to VG95319-102).
TACBEAM - 광섬유 커넥터 | Amphenol Socapex
암페놀 소카펙스의 tacbeam 광섬유 커넥터는 특수한 환경에서 사용할 수 있도록 설계된 자웅동체 커넥터입니다. 모노모드 및 멀티모드 옵션과 최대 4채널까지 지원하는 비접촉식 전송을 위한 광폭 패시브 기술을 기반으로 합니다. tacbeam 커넥터는 m83526/20 및 /21 인증을 획득하여 군용 및 산업용 ...
AFSI Achieves Qualification to MIL-DTL-83526 for its TACBeam® Connector ...
Allen, TX. July 2015 – FOR IMMEDIATE RELEASE –Amphenol Fiber Systems International (AFSI) is pleased to announce that its TACBeam® connector is qualified to the MIL-DTL-83526/20 & /21 specification. Approval to this standard makes it the best choice for harsh environment fiber optic ground-based applications around the world. Key features of the TACBeam®: Full qualification […]
AFSI Achieves Qualification to MIL-DTL-83526 for its TACBeam Connector
(AFSI) is pleased to announce that its TACBeam ® connector is qualified to the MIL-DTL-83526/20 & /21 specification. Approval to this standard makes it the best choice for harsh environment fiber optic ground-based applications around the world. Key features of the TACBeam ®: • Full qualification to the M83526/20 & /21 specification
ケーブルアセンブリー|アンフェノール・ソカペックス
施設 光ファイバーケーブル・アセンブリ. 当社の600 m 2の光ファイバーケーブル組立工場は、フランスのティーズにあります。 光ファイバーハーネスの組み立てには、研磨機、光学測定機、光学干渉計、光学制御システムなど、さまざまな機械を使用しています。
Amphenol
TACBeam ® Interface Adapter Amphenol Fiber Systems International, Inc. 1300 Central Expressway North, Suite 100 Allen, TX 75013 Phone: 214.547.2400 - 800.472.4225 Fax: 214.547.9344 Publication: AFSI-TACBeam ®IA-ds-091613. Specifications subject to change without notice. www.fibersystems.com - sales@fibersystems.com
电缆组件 | 安费诺 Socapex - Amphenol Socapex
电缆组件 根据您的需求定制. 客户的需求促使我们努力为军事和航空航天应用提供各种线束和电缆解决方案。我们深知每个项目都是独一无二的,因此我们能够根据您的需求设计和制造每种定制线束。
connector | Amphenol Global Search | Amphenol
6 Part 4: Assembly Process of Terminal and Cable 4.1: Applicable Cable Selection 4.1.1 Only suitable for the PV cable with cooper conductor. Tin coated wire of conductors is recommended. 4.1.2 The cable OD range from ø5.0mm to ø7.8m, the number of conductor strands is from 7 to 140 for 2.5/4.0/6.0mm² connector.