Search Results for thinkpad x1 extreme gen 5
Protimeter Speedy 2000 Series - amphenol-sensors.com
Moisture testers for soils, sands, powders, aggregates, concrete and masonry PROTIMETER Speedy ®
PROTIMETER Timbermaster - amphenol-sensors.com
after 5 minutes unless the default set-ting is changed (see section 3). 1 Using the Protimeter Timbermaster without the Temperature Probe The Timbermaster is calibrated for wood at 20°C (70°F). In general, tim-ber that is hotter than 20°C will give higher readings and timber colder than 20°C will give lower readings.
Telaire T9602 Humidity and Temperature Sensor for OEM Installation
T9602-5-D I2C Digital 5V 1.8m cable length T9602-3-D-1 I2C Digital 3V 1m cable length T9602-5-D-1 I2C Digital 5V 1m cable length T9602-3-A PDM Analogue 3V 1.8m cable length T9602-5-A PDM Analogue 5V 1.8m cable length T9602-3-A-1 PDM Analogue 3V 1m cable length T9602-5-A-1 PDM Analogue 5V 1m cable length AAS-920-638F - 06/2016 www.amphenol ...
SMP Female R/A to SMP Female R/A 12" Cable Assembly for .085 Cable
SV Microwave proudly presents the SMP Female R/A to SMP Female R/A 12" Cable Assembly for .085 Cable" 7012-0800 with push-on coupling type.
CUSTOMER DRAWING M - Amphenol Sine
Buchseneinsatz komplett (Kontakt Pin 5 vormontiert) female insert assembled (contact pin 5 pre-assembled) Endhülse end ferrule Wellschlauchadapter corrugated pipe adapter (M 2:1) (M 2:1) (M 2:1) AT62-12-0166 AT62-16-0822 für Wellschlauch NW23 for corrugated pipe NW23 Kontakte in separaten Beutel beigelegt contacts attached in separate poly ...
Contacto - kayeinstruments.com
Sobre Nosotros. Kaye & Amphenol; Kaye History; Medioambiente Sano y Seguro; Calidad; Términos y Condiciones; Novidad. Press Releases
PROTIMETER Timbermaster - amphenol-sensors.com
after 5 minutes unless the default set-ting is changed (see section 3). 1 Using the Protimeter Timbermaster without the Temperature Probe The Timbermaster is calibrated for wood at 20°C (70°F). In general, tim-ber that is hotter than 20°C will give higher readings and timber colder than 20°C will give lower readings.
2 Sensor for Automotive Applications - amphenol-sensors.com
• 4% to 6.5%: accuracy not specified • Temperature Dependence (outside 0C to 50C): +/- 0.5% of the reading Measurement and Sample Rate Characteristics: • Active Mode: 5 seconds sample rate • •Low Power Mode: 15 seconds sample rate • •Sleep Mode: 5 minute sample rate • Warm-up mode: 5 seconds after power up
Amphenol AAO/ACAD Product Compliance - Environmental Engineering
Amphenol AAO/ACAD Product Compliance - Environmental Engineering 40-60 Delaware Ave, Sidney NY 13838 Amphenol Aerospace Operations (AAO) and Commercial Air Division (ACAD)
Amphenol®
Via Barbaiana 5 1-20020 Lainate (MI) Italy Tel: +39 02 93254.204 Fax: +39 02 93254.444 Email: info@amphenol-aio.com Middle East: Amphenol Middle East Enterprises FZE Office C-37 PO Box 21107 Ajman Free Zone, UAE Tel: +9 716-7422494 Fax: +9 716-7422941 Email: jhussain@amphenol-industrial.com Asia: Amphenol Technology (Zhuhai) Co., Ltd.
NovaSensor NPP-301 Series Pressure Sensor - amphenol-sensors.com
NPP-301 Series Surface Mount Pressure Sensor Features • Low-cost surface mount package: SO-8 • Wide operating temperature range: -40°F to 257°F (–40°C to 125°C)
NTC Type B Series - amphenol-sensors.com
3 Type B Series Specifications Thermal Time Constant B05 • Still air at 77°F (25°C): 0.12 second • Plunge into water: 5.0 msec B07 • Still air at 77°F (25°C): 0.23 second
radsok-power-to-board-ptb-data-sheet-amphenol-industrial
Via Barbaiana 5 1-20020 Lainate (MI) Italy Tel: +39 02 93254.204 Fax: +39 02 93254.444 Email: info@amphenol-aio.com Middle East: Amphenol Middle East Enterprises FZE Office C-37 PO Box 21107 Ajman Free Zone, UAE Tel: +9 716-7422494 Fax: +9 716-7422941 Email: jhussain@amphenol-industrial.com Asia: Amphenol Technology (Zhuhai) Co., Ltd.
Psyclone™ Protimeter Thermo-Hygrometer Operating Manual
Protimeter Psyclone Page 5 Selecting Parameters and Calculation (cont.) • To select a calculation (Minimum, Maximum or Average): Scroll to the middle row, and then press the RIGHT or LEFT arrow key to select the desired calculation. The min/max/ave calculations are made from the last time the meter was powered up. If no parameter
PROTIMETER Timbermaster - amphenol-sensors.com
after 5 minutes unless the default set-ting is changed (see section 3). 1 Using the Protimeter Timbermaster without the Temperature Probe The Timbermaster is calibrated for wood at 20°C (70°F). In general, tim-ber that is hotter than 20°C will give higher readings and timber colder than 20°C will give lower readings.
P1300 Low Pressure Sensor Die - amphenol-sensors.com
All values measure a 25°C (77°F) and 1.5 mA excitation, unless otherwise noted. 2. Best fit straight line, 51314 ± 0.25% FSO 3. Typical between 0°C and 70°C (32°F and 158°F) 4. Die performance will vary depending on the die attach material. The die attach should be chosen to minimize the package stress transmitted to the
PRODUCT PORTFOLIO - svmicrowave.com
VSWR 2 MHz to 40 GHz 1.5:1 Max Axial Travel .079” Insertion Loss 2 MHz to 40 GHz .12 * √(f(GHz)) Radial Float ± .010” Cross Talk Requirement (dB MIN) 3 MHz to 30 MHz ≥ 140 dB Engage Force 3.5 lbs (typ) 30 MHz to 3 GHz ≥ 120 dB Disengage Force 3.5 lbs (typ) 3 GHz to 27 GHz ≥ 100 dB Min Pitch (.047”) .228”
Psyclone™ Protimeter Thermo-Hygrometer Operating Manual
Protimeter Psyclone Page 5 Selecting Parameters and Calculation (cont.) • To select a calculation (Minimum, Maximum or Average): Scroll to the middle row, and then press the RIGHT or LEFT arrow key to select the desired calculation. The min/max/ave calculations are made from the last time the meter was powered up. If no parameter
Application SpotlightApplication Spotlight
Telaire SM-UART-04L is a PM2.5 laser-based sensor that detects dust particle concentration in air by using an optical sensing method. A laser light emitting diode (LED) and a photo sensor are optically arranged in the device. The photo sensor detects the reflected laser LED light by dust particles in air.