Search Results for amphenol medical sensor solution filetype:pdf
NovaSensor NPC-100 and NPC-120 Disposable Medical Pressure Sensors
establishing and validating suitable process conditions to prevent damage to the sensor. NPC-100 and NPC-120 Series Specifications The NovaSensor NPC-100 and NPC-120 Series pressure sensor are specifically designed for use in disposable medical applications. The devices are compensated and calibrated per the Association for the Advancement of
T6743 CO2 Sensor Description - amphenol-sensors.com
T6743 Automotive CO2 Sensor 1. Introduction The T6743 from Telaire is an automotive qualified Carbon Dioxide Sensor that can be used in different configurations to meet customer needs for this type of sensor. Offering 3 operating modes, the sensor can monitor the cabin during Park, be used as a sensor for demand based ventilation systems in drive,
NovaSensor P165 3F Medical Silicon Absolute Pressure Sensor Die
All sensor wafers are electrically probed, visually inspected. All rejects are marked by an ink dot. Each wafer will be labeled with the lot number wafer number, device number and the number of available sensor die. Ordering Information Part Number Description 51564 2.5F, 300 mmHg Gage Warranty Amphenol Advanced Sensors warrants its products
Amphenol
The sensor clearance requirement for the device to allow the proper sensing. The sensor mounting features contain metal compression limiters. The sensor is designed to be mounted using M5 X 0.8 X 12 mm hardware with 11Nm maximum torque. Sensor orientation is not restricted but shall meet clearance specification above.
NovaSensor NPA Low Pressure Surface Mount Sensor Series
Pressure Sensor Series Amphenol Advanced Sensors. 2 Low Pressure NPA Specifications Parameter Value Units Notes Pressure Range 2 or 5 In H 2O 498 or 1245 Pa Maximum Overpressure 140 In H ... The NPA product series is provided in a miniature size as a cost effective solution for applications that require calibrated performance. Packaged in a ...
Pulse One Medical Cable Assemblies - amphenolalden.com
Amphenol Alden's pulseOne family of cable assemblies has been performance engineered to meet the challenges of medical instrumentation applications. Amphenol Alden connectors are typically preferred for the unmatched list of features and benefits that they bring to this demanding marketplace. Phone: 1(508) 427-7000 E-mail: Info@AmphenolAlden.com
NovaSensor P165 3F Medical Silicon Absolute Pressure Sensor Die
All sensor wafers are electrically probed, visually inspected. All rejects are marked by an ink dot. Each wafer will be labeled with the lot number wafer number, device number and the number of available sensor die. Ordering Information Part Number Description 51564 2.5F, 300 mmHg Gage Warranty Amphenol Advanced Sensors warrants its products
Thermometrics GE-1711/GE1797 Engine Temperature Sensors
5% salt solution at 95°F for 500 hours. Dry for 1 week. After the test, sample must be torn down. No water entry permissible, must meet standard performance requirements Water Immersion Stabilize part at 190°F. Immediately immerse in 32°F solution of paint and water for 35 minutes. Rotate part 180° after 10 minutes and 90° after an
Thermometrics temperature sensor solutions - amphenol-sensors.com
Amphenol Advanced Sensors portfolio of sensor-based solutions. Thermometrics pioneered lead frame technology, unifying the probe terminal and thermistor lead into a single constructed metal substrate. This innovation was the building block to today’s fully automated volume production process, which ensures the highest degree of
NovaSensor NPC-100 and NPC-120 Disposable Medical Pressure Sensors
establishing and validating suitable process conditions to prevent damage to the sensor. NPC-100 and NPC-120 Series Specifications The NovaSensor NPC-100 and NPC-120 Series pressure sensor are specifically designed for use in disposable medical applications. The devices are compensated and calibrated per the Association for the Advancement of
NovaSensor P165 3F Medical Silicon Absolute Pressure Sensor Die
All sensor wafers are electrically probed, visually inspected. All rejects are marked by an ink dot. Each wafer will be labeled with the lot number wafer number, device number and the number of available sensor die. Ordering Information Part Number Description 51564 2.5F, 300 mmHg Gage Warranty Amphenol Advanced Sensors warrants its products
Application SpotlightApplication Spotlight - amphenol-sensors.com
Title: Themometrics Temperature Sensing in Medical Devices Author: Amphenol Advanced Sensors Subject: Medical applications demand the ultimate in accurate and reliable monitoring of critical temperature measurement.\nFrom the Amphenol Advanced Sensors family of brands, Thermometrics, Inc., designs and manufactures an extensive line of NTC thermistors and \ non-contact infrared \(IR\) based ...
NovaSensor P165 3F Medical Silicon Absolute Pressure Sensor Die
All sensor wafers are electrically probed, visually inspected. All rejects are marked by an ink dot. Each wafer will be labeled with the lot number wafer number, device number and the number of available sensor die. Ordering Information Part Number Description 51564 2.5F, 300 mmHg Gage Warranty Amphenol Advanced Sensors warrants its products
NovaSensor P165 3F Medical Silicon Absolute Pressure Sensor Die
All sensor wafers are electrically probed, visually inspected. All rejects are marked by an ink dot. Each wafer will be labeled with the lot number wafer number, device number and the number of available sensor die. Ordering Information Part Number Description 51564 2.5F, 300 mmHg Gage Warranty Amphenol Advanced Sensors warrants its products
NovaSensor P165 3F Medical Silicon Absolute Pressure Sensor Die
All sensor wafers are electrically probed, visually inspected. All rejects are marked by an ink dot. Each wafer will be labeled with the lot number wafer number, device number and the number of available sensor die. Ordering Information Part Number Description 51564 2.5F, 300 mmHg Gage Warranty Amphenol Advanced Sensors warrants its products
NovaSensor P1602 Pressure Sensor Die - amphenol-sensors.com
P1602 is available as an absolute pressure sensor, where the applied pressure is referenced to an internal vacuum sealed within the die. With NovaSensor’s Senstable® process, the P1602 will provide very low long-term stability errors and excellent repeatability. Amphenol Advanced Sensors
2 Sensor for Automotive Applications - Amphenol
Internal CO2 Sensor Specifications General Performance: ABC Logic This sensor implements an algorithm to self-calibrate to its ambient environment. The sensor uses readings during fresh air conditions to make the correction. ABC Logic corrects for a variety of use factors including transitions to new environments, change in altitudes, mishandling
2023 - Amphenol
4 2023 SSTAINABILIT REPORT AMPHENOL CORPORATION About Amphenol Amphenol Corporation is one of the world’s largest providers of high-technology interconnect, sensor and antenna solutions. Our products Enable the Electronics Revolution across a diverse array of end markets. We are a global company, with
Telaire T6743 Automotive CO2 Sensor - Amphenol
Amphenol Advanced Sensors T6743 Automotive CO2 Sensor Overview The Telaire® T6743 is an automotive-qualified CO2 sensor for in-cabin applications. • Ventilate the cabin space providing automatic fresh air, aiding driver alertness • CO2 leak detection in the cabin space in vehicles using CO2 refrigerant HVAC systems
130+ DIVISIONS Amphenol: Empowering Connectivity Worldwide
Amphenol: A Global Connectivity Leader Amphenol, headquartered in Connecticut, is a world leader in interconnect, sensor, and antenna solutions. With a presence in 70 countries and 130+ divisions, we redefine connectivity. Our Unique Business Model: Empowering Your Success Amphenol's 130+ divisions operate independent-