Search Results for marport extract data
Extracting Data from SDS Files - marport.com
You can extract data contained in SDS files and display the contents in a table on a spreadsheet application, using Marport sds2txt application. Ask your local Marport office for more details about ...
Scala User Guide - Marport
Scala is Marport’s advanced trawl monitoring system that collects, processes, stores and displays data sent from multiple sensors, sounders and other connected devices. It gives the user full control over its fishing operations.
Scala2 User Manual - Marport
Scala2 is Marport’s advanced trawl monitoring system that collects, processes, stores and displays data sent from multiple sensors, sounders and other connected devices. It gives you full control over the fishing operations. In order to suit the working conditions, gear and sensor data type available, this monitoring system
Recording and Replaying Data - marport.com
Read this section to know how data are displayed on Scala and how to change their display. Recording and Replaying Data Data received by Scala can be replayed with Scala Replay application.
Recording of Incoming Data - marport.com
Read this section to know how data are displayed on Scala and how to change their display. Recording and Replaying Data Data received by Scala can be replayed with Scala Replay application.
M4 and Mx Computer System - Marport
Marport software application collecting, processing, storing and displaying data received from sensors, sounders and other connected devices. Marport software application replaying data recorded in Scala2.
Replaying Data on Scala Replay - marport.com
Read this section to know how data are displayed on Scala and how to change their display. Recording and Replaying Data Data received by Scala can be replayed with Scala Replay application.
Marport
Marport designs and manufactures catch control and net monitoring sensors, echo sounders, current profilers and sonar for the world's fishing fleet.
M3 & M5 Systems User Guide - Marport
• You can have a simultaneous reception from up to 12 data (depth, pitch, roll...) from standard sensors (e.g. door spread, catch). • You can combine standard sensors with 1 high-definition reception sensor (e.g. HDTE or NBTE
User Guide MANUAL - Marport
There are 2 NMEA and 4 NTC entries to receive hydrophones' temperature data. Important: To ensure proper and safe use of this equipment, carefully read and follow the instructions in this manual.
Introduction - Marport
Compare data from equivalent sensors using multiple history plots. Moreover, a key feature of Scala is that it is designed to meet tomorrow’s requirements: It incorporates 3D simulation with bathymetry using a simple GPS data connection. It has a range of standard data inputs and outputs.
Sensor Data - Marport
Sensor data is raw or filtered data received from the sensors. By default, the location of the sensor on the trawl gear is written between brackets next to the sensor name. To know to which location the number corresponds, refer to the pictures in Sensor Nodes. Blinking green: data is received.
Outputting NMEA Data to Other Systems - marport.com
Click Menu > Settings. In the NMEA Outputs tab, click Add. Choose the type of connection between serial port, UDP or TCP socket. Enter the output parameters. Serial port: select the name of the port and baud rate of the device. UDP: enter the port number from which data are broadcast.
Receiver Data - marport.com
Receiver Data Using the Virtual Charger Room You can display the fleet of sensors in Scala2 Virtual Charger Room , when sensors are connected to the Dock or trawling.
Outputting NMEA Data to Other Systems - marport.com
Under the Data to Emit tab, select which data you want to output: Select Emit Sensor Data to output data that is received on Scala2 from Marport sensors, with or without filters.
Trawl Positioning System - Marport
Watch these short videos to learn how to use Marport sensors. Learn how to configure the sensor settings. Learn how to configure the receiver to be able to receive and display door sensor data. Learn how to install door sensors on the trawl gear. Read this section for troubleshooting and maintenance information.
Adding NMEA Data from External Devices - Marport
You can display on Scala data received from external devices such as GPS, sonar, winch control system, compass or anemometer.
Connecting External Devices - Marport
Marport Mx systems are able to receive data from external devices such as GPS, sonar, winch control system, compass or anemometer. These data can be displayed in Scala2 software. This can help you improving the system performance.
CatchNavigator UserManual en V1 - Marport
Marport's Catch Navigator tells you when your trawl starts to fill. Placed on the top of the trawl codend, it monitors the amount of catch that you have and warns you when the trawl is full. You can even use it to determine a precise amount of fish inside the trawl net.
Displaying the MultiDepth View - Marport
You can display data from A2S door spread sensors on a 3D view of the trawls and doors.