Search Results for marport extract data
Adding Events - marport.com
You can mark a specific moment when receiving live data to find it back when replaying data with ScalaReplay2. Display Configuration. Read this section to know how data are displayed on Scala2 and how to change their display. Control Panels. Customization Panels.
Connecting External Devices - Marport
Marport Mx systems are able to receive data from external devices such as GPS, sonar, winch control system, compass or anemometer. These data can be displayed in Scala2 software. This can help you improving the system performance.
Marport Compact System
Marport Compact | V4 | Legal Legal History V1 03/30/22 First release V2 04/26/22 • Added topics in Troubleshooting on page 37. ... • Added guidelines for the Up sounding mode in Data Display Options on page 27. • Clarified guidance in Changing the Model of Trawl Doors on page 32.
USER MANUAL - marport.com
and Catch Explorer Pro are part of Marport’s latest generation of sensors. They have been designed as a direct replacement for older versions, offering enhanced features, unavailable in previous models. These enhancements include compatibility with the latest Mosa2 and Scala2 software features, and with the Dock smart charger. Marport
Introduction - Marport
Scala2 is Marport’s advanced trawl monitoring system that collects, processes, stores and displays data sent from multiple sensors, sounders and other connected devices. It gives you full control over the fishing operations. In order to suit the working conditions, gear and sensor data type available, this monitoring system offers unparalleled flexibility and is easily configurable.
Data in Scala2 is wrong - marport.com
Data displayed in Scala2 is wrong. For sensors with echograms, the echogram is noisy. There are signal interferences. First, check that the sensor frequencies and telegrams are the same in the sensor ...
Data in Scala2 is wrong - marport.com
Data displayed in Scala2 is wrong. For sensors with echograms, the echogram is noisy. There are signal interferences. First, check that the sensor frequencies and telegrams are the same in the sensor ...
Spread Sensors Pro - marport.com
Adding Data from External Devices 58. Receiving Warp Lengths from Scantrol 61. Configuring Data Display on Scala2. 63. Displaying Trawl Door 3D View. 63 Using the . MultiTrawl View on Scala2 67 Displaying Door Positioning Data. 74. Changing the Number of Trawls. 77
Introduction - Marport
Marport 's Catch Navigator tells you when your trawl starts to fill. Placed on the top of the trawl codend, it monitors the amount of catch that you have and warns you when the trawl is full. ... Optionally, it can also track pitch, roll, depth, height and temperature data. Our latest model offers enhanced robustness, extended battery life, and ...
Marport
Displaying Spread Plot for Twin Trawls. Play. 02:38
Data in Scala2 is wrong - marport.com
Data displayed in Scala2 is wrong. For sensors with echograms, the echogram is noisy. There are signal interferences. First, check that the sensor frequencies and telegrams are the same in the sensor ...
Configuring Data Display - marport.com
Data title should be: Spread Master / Spread Slave / Spread Clump for Spread sensors. Door Sounder; The title is followed by the node where the sensor was placed when added to the system. Data displayed (e.g. spread distances, pitch & roll) depends on the firmware installed.
Technical Specifications - Marport
Uplink frequency 30 to 60 kHz Range to vessel up to 2500 m* Data update rate Trident Down Looking Down only: Ranges from 20 to 160 m: Echogram, temperature, depth, pitch, roll ... / **Marport Standard Marine Limited Warranty. The housing is delivered with 4 soft shackles: dimensions 7-10x100x100 mm, resistance up to 1 ton (+/- 10% tolerance). ...
Introduction - Marport
Marport’s Trawl Explorer is your eye on the fishing gear. This sounder can be placed on your trawl headrope or tunnel in order to send useful information to the wheelhouse. ... Depth data; Temperature data; Pitch and roll data; Distance from the sensor to the seabed or footrope;
Data in Scala2 is wrong - marport.com
Data displayed in Scala2 is wrong and the echogram is noisy . There are signal interferences. ... Charge the sensor at any battery level with either Marport Dock charger, Basic Sensor Charger or Medusa II Multi-charger. Cleaning the Sensor. You need to regularly clean the sensor for proper performance. ...
Introduction - Marport
Here are examples of data received by the Trawl Navigator in Scala2. Safety Guidelines. Read this section before using the product. Description. Introduction. Marport's Trawl Navigator is a high-definition net sounder, designed to operate on the trawl headline. It is suited for bottom trawling and will offer better performance on trawls with a ...
Data in Scala2 is wrong - marport.com
Data displayed in Scala2 is wrong. There are signal interferences. First, check that the sensor frequencies and telegrams are the same in the sensor configuration (via Mosa2 ) and the receiver ...
Marport
dcaute@marport.com Didier graduated from the Ecole Polytechnique de l'Université de Nantes, France in 1996 with a degree in Electronic Engineering and Computer Science. He was employed as a consultant design engineer with EchoPilot Ltd. in England, where he developed forward looking sonar technologies and products.
Introduction - Marport
Marport's Speed Navigator is a high-definition net sounder ... It also tracks pitch, roll, depth and temperature data. The high-definition echogram images allow you to see fish passing through the trawl and have an overview of the trawl opening. In order to efficiently follow the trawl descent, echogram ranges are configurable from 5 to 160 ...
Data in Scala2 is wrong - marport.com
Data displayed in Scala2 is wrong. For sensors with echograms, the echogram is noisy. There are signal interferences. First, check that the sensor frequencies and telegrams are the same in the sensor ...