Search Results for marport extract data
Main Parts - Marport
Examples of data received and displayed in Scala2 application. Safety Guidelines. Read this section before using the product. Description. System Compatibility. The Catch Navigator is compatible with the following versions of Marport 's software and equipment. Firmware and Features. This section describes the ...
Outputting NMEA Data to Other Systems - marport.com
TCP: enter the port number from which data are sent. Under the Data to Emit tab, select which data you want to output:. The first two options output data that are received on Scala from Marport sensors.; Select Emit trawl positioning sentence if you need to send positioning data to another system (such as a cartography software) and choose the sentence corresponding to this system.
SpeedNavigator UserManual en V1 - marport.com
Range to vessel; up to 2500 m* Data update rate • 5-meter range: Echogram @0.16 s - temperature, depth, pitch, roll, battery level, along speed, across speed @8.07 s
User Guide MANUAL - Marport
The Mx computer processes the signal and displays the data on a screen connected to the Mac. You can configure the sensors and display data to suit your ... Mosa2 on a tablet computer: refer to Marport sales offices to know the recommended model. Software. Software Application Name. Definition. Marport . validated MacOS. Operating system on ...
Seine Sensors User Manual - marport.com
• Replaced DealerWeb website by Marport Authorized Service Provider (MASP). • Added contact details of the sales office in United Kingdom, and updated contact details of Iceland sales ... Data update rate Depth: 1-8 sec. - Temp: 3-16 sec. - Height: 1-14 sec. Depth range up to 1800 m
Trawl Explorer User Guide - marport.com
Marport’s Trawl Explorer is your eye on the fishing gear. This sounder can be placed on your trawl ... • Depth data • Temperature data • Pitch and roll data • Distance from the sensor to the seabed or footrope The Trawl Explorer can adapt to different types of fishing methods. For example, you can fully
Door Sensors User Guide - Marport
Tip: Click Marport logo at the bottom of pages to come back to the table of contents. Introduction Door sensor family includes two types of sensors: Spread Sensor and Door Sounder. ... then sends distance data to the vessel. Sensors also monitor pitch and roll, water temperature and depth. This gives you a
Receiver Data - marport.com
You can be alerted by an alarm when data received have a given value. Changing the Default Units. You can change the default units of data displayed in Scala. Recording and Replaying Data. Data received by Scala can be replayed with Scala Replay application. Receiver Data.
Connecting the Sensor to Mosa2 - Marport
You need to check the orientation of the A1 board inside the sensor in order to correctly receive data. Canceling the Ringing. On NBTE V2 echograms, there is a ringing coming from the transducer, that appears as a red line on top of the echogram. You can cancel it. ...
Sensor Data - Marport
Sensor data is displayed in the Control Panels on the right side of the screen. Sensor data is raw or filtered data received from the sensors. By default, the location of the sensor on the trawl gear ... Back to support page. Jump to main content Scala. V. 01.06.34 Index. Search. Home; Display Configuration ...
Technical Specifications - marport.com
Catch Sensor Uplink frequency 30 to 60 kHz Range to vessel up to 2500 m* Depth range up to 1800 m Data update rate Catch full: 20 sec. - Catch empty: 30 sec. - Depth: 3-8 sec ... / † Depends on sensor uplink power and options. / ‡ Based on average charging time. / **Marport Standard Marine Limited Warranty. Catch Explorer Beamwidths ...
USER MANUAL - Marport
Marport is a division of Airmar Technology Corporation. Disclaimer. Marport . ... The Mx computer processes the signal and displays the data on a screen connected to the Mac. You can configure the sensors and display data to suit your needs. The . M3 PRO has a full range of capabilities:
Introduction - marport.com
Data received can be recorded on a built-in SD card and replayed in higher definition. They can be installed on port, starboard doors and clumps. ... They are compatible with Marport Dock product, with which you can easily charge, monitor, configure and update the connected sensors (up to 4). A Door Sensor SC is also available, designed to work ...
Echogram Display Settings - Marport
The scope displays the latest received sonar data. Set VRM: Sets a range marker at a given depth. Draw Bottom Line: Displays a yellow line at the bottom of the trawl and a white line at the beginning of the seabed. ...
Introduction - marport.com
Catch sensor: gives you the catch status of the trawl (empty or full), along with depth, water temperature and pitch and roll information. Catch sensors can emit on a single frequency of 40 kHz (Marport, Scanmar) or 70 kHz (Simrad, Wesmar), or on a dual frequency (40 kHz/70 kHz).; Catch Explorer: gives you the catch status of the trawl, with depth, water temperature and pitch and roll information.
SCALA2 Iceland South Africa USA Spain - Marport
Iceland Marport EHF Fossaleyni 16 112 Reykjavík, Iceland supporticeland@marport.com USA Marport Americas Inc. USA 12123 Harbour Reach Drive Mukilteo, WA 98275 USA supportusa@marport.com France Marport France SAS 8, rue Maurice Le Léon 56100 Lorient, France supportfrance@marport.com
Speed Sensors User Guide - marport.com
• Replaced DealerWeb website by Marport Authorized Service Provider (MASP). • Added contact details of the sales office in United Kingdom, and updated contact details of Iceland sales ... Here are some examples of data received from Grid, Trawl Speed and Speed Explorer sensors and displayed in Scala/Scala2. Grid sensor display 1. Control ...
Installing Sensor Pockets - Marport
Cut round openings in the doors. Place the sensor pocket with the bottom portion sticking out of back side of the door. Adjust accordingly to the elevation angle and angle of attack you need (see Pocket Angle of Attack).Picture below shows angles of attack seen from above the door.
MARPORT DOOR QUICK REFERENCE GUIDE
Marport EHF Tónahvarf 7 203 Kopavogur, Iceland supporticeland@marport.com South Africa Marport South Africa Cape Town, Western Cape, 11 Paarden Eiland Road, Paarden Eiland, 7405 csanter@marport.com France Marport France SAS 8, rue Maurice Le Léon 56100 Lorient, France supportfrance@marport.com Offices Norway Marport Norge A/S Breivika ...
Configuring Data Display on Scala2 - marport.com
Open the customize panel, then go to Mx and drag Door 3D View to the page.; To change the door or clump model: From the top left corner, click Menu > Settings.; Click the Trawl tab and select the models of doors and clump from the lists, using left and right arrows.; You can also change the viewing angle: looking from the trawl toward the vessel (front), or from the vessel toward the trawl (back).